在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
新闻中心

          业务资讯

          07/09/2005

          Schneider Electric, customers solutions on display !



          Schneider Electric has just signed a contract with STAR Madagascar. Created in 1953, STAR is the largest producer of mineral and fizzy drinks in Madagascar and have four production sites located in: Andraharo, Antsirabe, Diego-Suarez and Andranovelona.

          In order to face up to an increase of the consumption (more than 30 % in 3 years), Star Madagascar embarked on a renovation program for its production installations and equipment. As far as the electrical installation was concerned, this program covered the replacement of the main and secondary substations at the four sites. The installed power has thus been increased.

          For this project, Schneider Electric supplied the medium voltage equipment (main and secondary substations, MV/LV transformers) and the Main Low Voltage Switchboards. Schneider Electric also ensured maximum availability and helped in the choice of architecture, installation supervision (sub-metering) in partnership with Someca, the local contractor.