在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
新闻中心

          业务资讯

          29/06/2006

          A complete and unique solution which guarantees overall quality.

          Sugar production has experienced in Mexico - 7th largest producer in the world, strong consumption growth in recent years. And sugar producers want to use in their plant the best and the newest technology.

          To help with sugar production improvement, Schneider Electric Mexico supplied a global solution for a sugar mill plant in Tala, a town situated in the east centre of the country.

          Modernize and make more efficient the sugar production processes, reduce operation costs, lower the index of failure, improve the quality of final product... Several objectives handled with Schneider Electric automation system.

          “We also made several commitments to our customer: feasibility of communication with our equipment, collaboration with a local distributor, on-time delivery, overall quality…,” explains Ismael Gonzalez, West Sales Industry Manager, Schneider Electric Mexico.

          A global and unique solution
          The automation system handles the whole process, using a supervising system and communication between equipment. The supervision, made from one local point, allows to see parameters of functioning at the plant, change directly on line parameters of production and have feedback on the equipment state.

          - Square D S2 substation
          - 3 Federal Pacific switchboards in Nema 3R enclosure,
          - 1 starter in MV for 500 HP / 4160 V,
          - 10 Himel enclosures with Telemecanique control equipment and Square D molded case circuit breakers,
          - 36 ATV 71 variable speed drives ATV 71 and 24 ATS 48 solid state starters ATS 48.

          More information :