在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
新闻中心

          业务资讯

          31/08/2006

          The new artificial island will soon welcome its first visitors


          The Palm, Jumeirah, is the name given to a new resort situated off the coast of Dubaï.


          This new ultimate holiday destination is equipped by Schneider Electric. It already provided the medium and low voltage distribution equipment: 72 substations are operating power for buildings and villas. And it also supplied 2,000 starters for swimming pool control panels.

          The complex, said to be visible from the moon, will be a retreat, a quiet, serene and safe haven for living, leisure and relaxation.

          The Palm, Jumeirah will provide an outstanding array of retail and lifestyle options for residents and tourists to enjoy, creating a new center for Dubaï. It will offer the world’s most exclusive brands, and an array of boutiques and restaurants.

          The first residents are expected to arrive by the end of the year.

          The Palm, Jumeirah, in Figures
          - First island in the Palm trilogy
          - 5km in length, 5 km in width