在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
新闻中心

          业务资讯

          20/09/2006

          Eisai Research Institute will use TAC system at new Boston area research facility


          “A unique workable solution” was proposed by TAC for Eisai Research Institute new facility.

          Eisai Research Institute, a U.S. pharmaceutical company, through a general contractor, has awarded to TAC, a company of Schneider Electric, the contract for integrated building automation and security systems at their new Research Center in Andover, Massachusetts, USA.

          The building automation system (BAS) project includes an integrated laboratory airflow control system. In addition to the integration of TAC’s Andover Continuum™ for the BAS and security operations, the new building includes seven direct digital controlled air handlers, two chillers, two cooling towers and four boilers, all of which will be controlled via BACnet® interfaced to Andover Continuum.

          “The highly flexible Andover Continuum software enabled our team to propose a unique workable solution,” said David Berardi, vice president Systems Integration-East, TAC.

          > More information on Eisai:
          Eisai Inc. is the U.S. pharmaceutical subsidiary of Tokyo-based Eisai Co. Ltd. The Eisai Research Institute, which will expand existing operations into the new building, conducts discovery research on complex synthetic and organic chemical compounds. Accordingly, more than 60 percent of the new 150,000-square foot facility will be dedicated to research laboratories.

          More information :