在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
新闻中心

          业务资讯

          23/03/2007

          Energy costs savings and maximum productivity, the energy and automation infrastructure answers all needs of Aliaga Organized Industrial Region


          During the official opening of the Organized Industrial Region of Aliaga, Turkish government, represented by Prime Minister, Recep Tayyip Erdogan, awarded Schneider Electric with a thanking plaque, given to Turhan Turhangil, Turkey Country Manager.

          For this project, which started in 2005, Schneider Electric realized the medium and low voltage infrastructure for the whole industrial region as well as provided automation and Scada technologies (supervision, control and data acquisition).

          The system provides safe and quality electric use. It also help obtain maximum productivity with optimum energy consumption and uninterrupted operation capability. A must for all productive companies situated in the Industrial Region of Aliaga.

          Located next to Izmir, Aliaga Organized Industrial Zone is one of the main centers of manufacturers, exporters and importers in Turkey. “The infrastructure quality is very important, states Turhan Turhangil. In a major production area, it is necessary for the companies which operate in these industrial regions to make production more economically, decreasing their costs of energy.”

          It is then necessary for the companies making production in Organized Industrial Regions to have specific advantages in infrastructure : “We established the system by taking into consideration this principle. We combined savings with our energy policy which is continuous and 100% quality.”

          More information about Schneider Electric in Turkey: