在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
新闻中心

          业务资讯

          28/05/2007

          With Ilevo, broadband communication to all your power outlets


          Power Line Communication (PLC) specialist within Schneider Electric, Ilevo proposes its expertise of 200 Mbps PLC technology to the general public, including professionals, with a new In-home offer intended for home and small offices applications.

          “The In-home segment is booming, explains Xavier Pain, Vice-President for In-home market.To respond to this market infatuation – estimated volumes of about 500.000 PLC products sold in Europe in 2007, and over 1 million in 2008 – there are many competitors, worldwide. As a matter of fact, Ilevo relies on synergies with other activities within Schneider Electric to develop original offers and bring a global solution to end-users.”

          Broadband access into every electrical socket of your home

          The first product of this new offer, called <ILV7 serie>, is the ILV701 PLC Ethernet Adapter. It allows to set-up an Ethernet bridge between two multimedia devices, via the electrical network. It also offers the simplest solution to create its local IP network and bridge ISP services everywhere, to all multimedia equipment: no new wiring, no installation works, no configuring, no microwaves.

          And to complete its services, Ilevo has chosen adapted business models, such as direct online sales. Available online since more than a month, Ilevo e-shop (e-commerce website) offers to Internet surfers the best of PLC at outlet prices.

          For more information on Ilevo: