在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
关于我们

          公司新闻

          01/07/1999

          Le Mistral, the latest French-built cruise ship, is equipped with many Schneider Electric products

          Le Mistral, the latest vessel to come out of France’s Chantiers de l’Atlantique shipyards, was inaugurated on June 25. More than 12,000 people attended the ceremony, including French Prime Minister Lionel Jospin. Le Mistral continues a nearly 40-year tradition that began with the legendary ocean liner France. The 216-meter-long beauty is equipped with four 5,650 kWh diesel engines that supply all the onboard current. Schneider Electric provided electrical distribution products and switchgear for the project. The package included two Merlin Gerin Masterbloc MB300 low voltage switchboards, Merlin Gerin Masterpact (5,000 A) and Compact NS circuit breakers, Telemecanique AK3 multi-connection busbar trunking for motor starters, a number of Telemecanique industrial control products (buttons, lights, contactors, D2 and F series relays) and thecelebrated Integral contactor-breaker. Schneider Electric has worked with the shipbuilding industry for more than 60 years. The Company was called in on the project by Chantiers de l’Atlantique subcontractor Ateliers de Montoir in recognition of this expertise. Le Mistral is now on its way to the Mediterranean Sea, and it will sail to the Caribbean this winter.

          Le Mistral facts and figures
          Length: 216 meters
          Width: 29 meters
          Weight: 48,000 metric tons
          Cruising speed: 19.5 knots
          Top speed: 21.5 knots
          Onboard current: supplied by four 5,650 kWh diesel engines
          Area open to the public: more than one hectare
          Glass: more than 2,000 square meters
          Capacity: 1,200 passengers
          Cabins: 600 (400 overlooking the sea), including 80 luxury cabins with balcony
          Crew cabins: 270 for the 500 crew members