在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
关于我们

          公司新闻

          01/10/1999

          A new software for OEMs and panelbuilders

          Telemecanique Tego Power Design is a new software forconfiguring motor starters (Telemecanique GV2 circuit breakers and K&D contactors) using the Tego Power installation solution. Tego Power Design allows machine builders and their panelbuilders to select the motor starter components to be installed without risk of error. The product saves time, enhances safety and makes it possible to update components. It also offers a whole range of useful functions, including the ability to memorize configurations, define and print front facing labels, and print and forward parts lists and invoices. The Tego Power Design CD-ROM is now available in French and English. A similar software package exists for the Tego Dial range. For more information on Tego Power Design, call your Schneider Electric contact today or get in touch with our local subsidiary via our website—just click «Get to know us» and then «An international organization».

          Telemecanique Tego Power was awarded the prize for innovation at the Intel 99 tradeshow in Milan, Italy.