在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
关于我们

          公司新闻

          01/09/2000

          Touch’n Click HMI combines safety and innovation

          Touch’n Click is the latest generation of Telemecanique Magelis graphic HMI terminals for automated installations. This particularly innovative solution is based on a technology that combines the comfort of pushbuttons with the flexibility of touchscreens. Touch’n Click’s transparent, mobile keys are attached to the terminal’s touchscreen, thereby eliminating the risk of slippage when the operator makes a selection. The unit’s design also clearly separates the viewing/adjustment area from the control area. Touch’n Click extends the currentMagelis lineup of keyboard and touchscreen terminals and uses Magelis’ XBTL 1000 configuration software.

          For further information, please contact your Schneider Electric representative.