在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
关于我们

          公司新闻

          01/08/2001

          TeSys recognized

          Mesures, the leading French trade magazine specializing in industrial control, automation and instrumentation, has compensated TeSys in awarding it the Technology Prize in the "automation and actuators" category.
          The Telemecanqiue TeSys range is composed of circuit breakers, contactors and thermal overload relays ensuring motor starter and protection functions, up to power of 75 kW.
          The jury was particularly impressed with the Quickfit solution and the spring connector system enabling motor starters to be implemented without the use of wiring or tools.