在菜单中选择您的国家或地区,或在世界地图上点击选择 *
Country Selector Alternate Image
关于我们

          公司新闻

          01/02/2004

          Geronimo turns back to Brest

          After breaking its second gennaker (a foresail for light and medium winds) on Friday, February 13th, Geronimo was forced to return to Brest. Olivier de Kersauson and his crew plan to re-embark in 6 days' time after spending 3 days at the sailmaker's for repairs. The trimaran will then once again cross the starting line as soon as new window opens in the weather.
          Geronimo had taken three new gennakers with it. The first broke right at the start and the second then broke in the same way on Friday. As the third was identical, its theoretical reliability was low. ODK and his two deck officers decided not to risk breaking another one before even crossing the Equator.