成功案例: 石油天然气
Fos Cavaou LNG Terminal (France)
 | | Availability better than 99,977%, Overall target unreliability < 1 occurrence/year |
I. CUSTOMER ENVIRONMENT / PROJECT CONTEXT
Customer profile:
- Consulting Engineering for all fields relating to Natural Gas. In partnership with foreign companies, it was responsible for the new liquid natural gas terminal designed to provide 8 billions m3 of Natural Gas per year with a storage capacity of 330,000 m3 in 3 reservoirs.
Customer objective and constraints:
- Validate the electrical distribution network architecture to show that availability and reliability targets for the process have been met, taking into account:
- Load sensitivity
- Futur network expansion
- Equipment maintainability
II. SOLUTION IMPLEMENTATION
Implementation methodology (main phases):
- Electrical Distribution Network Reliability Study
1. Understand and identify risks
2. Optimize architecture, compare solutions, highlight weak points
3. Design redundancies and back-up configurations
4. Optimize maintenance plan
Solution overview (services, products, systems, architectures...) :

III. RESULTS / ACHIEVEMENT
Customer benefits:
- Loss of gas emission on distribution & transport network :
- Overall target unavailability < 2 hours per year; P(t) < 2,28.10-4; Availability better than 99,977%
- Overall target unreliability < 1 occurrence per year; λeq (t) < 1,14.10-4 /h
Schneider Electric differentiating values VS competitors:
Target availability and reliability are achieved thanks to:
- Taking into account dependability issues from the early stage of the project
- Redundancy implemented at architecture level
- Automatic reconfiguration
- Process equipment dispatching
- Failure detection system