技术常见问答

询问问题

Adjust values of the time delay fro XPS-AT Emergency stop monitoring delay output.

the time delay adjustment Mean to outputs 57/58 and 67/68 for XPS AT . Adjustment by a 12 position selector switch located in the front cover, Positions of adjustment (in secondes) : 0 - 0.5 (min value) - 1 - 2 - 4 - 6 - 8 - 10 - 15 - 20 - 25 - 30 (max value).

对您是否有帮助?
我们如何进行信息改进?