技术常见问答

询问问题

The substitutes of GEZ safety module for use with two-hand control unit.

GEZ safety relay accessed to type III-B according to EN 574. for two-hand control XY2-SB. It does not have complete equivalent in the XPS range. XPSBC is the most suitable replacement in press applications .

对您是否有帮助?
我们如何进行信息改进?