技术常见问答

询问问题

How can I changing the item displayed on ATV21?

Please refer to the following table:

 

Parameter

Choice :

 Description :

code :

 

 

F710

0

 Operation frequency in Hz (factory setting).

 

1

 Frequency command in Hz

 

2

 Output current in % or Amper (1).

 

3

 Inverter rated current in Amper.

 

4

 Inverter load factor in %.

 

5

 Output power in kW.

 

6

 Frequency command after PID-regulator (Hz).

 

8

 Output speed in rpm.

(1) : Factory setting is Amper. Can be changed to % > Parameter F701 = 0
对您是否有帮助?
我们如何进行信息改进?