技术常见问答

询问问题

What is the pin out of the Powersuite cable ?

There are two exist cables for Powersuite. The physical difference between the cable before and after 09/2001 is on the connector.
Pin out of the cable Powersuite before 09/01 (cable used for ATV28 before 09/01) :
Drive PC
RJ45 Subd9

1 – nc
2 – 0 V ------------------------ 4
3 – D(B) ------------------------ 7
4 – nc
5 – D(A) ------------------------ 3
6 – nc
7 – 10v ------------------------ 6
8 – nc


Pin out of the Powersuite cable between the drive (or the softstarter) and the PC :
Drive PC
RJ45 Subd9

1 – nc
2 – nc
3 – nc
4 – D(B) ------------------------ 7
5 – D(A) ------------------------ 3
6 – nc
7 – 10v ------------------------- 6
8 – 0v ------------------------- 4
 
对您是否有帮助?
我们如何进行信息改进?