技术常见问答

询问问题

【外部】【Vijeo Citect 基本配置】 Citect与三菱PLC通信时,端口与板的设置该注意些什么?

Board Name: Board1
Board Type: TCPIP
Address: 0

Port Name: Port1_Board1
Board Name: Board1
Special Opt: -i192.168.0.21 -P1025 -T (IP address of the PLC)

IODevice Name: IODeviceName
Address: 255
Protocol: MELSCNET1
PortName: Port1_Board1

对您是否有帮助?
我们如何进行信息改进?