Certification Manager – Connected Offer
位置:
上海 (上海), 中国
类别:
市场
Req ID:
007VL6
工作描述
- Evaluate the conformity of the offer according standards and other statutory requirements
- Ensure the collaboration and knowledge sharing within (and sometimes beyond) Energy Management
- Coordination with Notified Bodies
- Support the Customer Satisfaction & Quality Team in case of a critical non- conformity
资格
- Knowledge in conformity assessment for connected offer in international market
- Knowledge in application of European Directives (Blue Guide C272, RED 2014/53/EU etc.)
- Experience in Communication Interfaces and protocols
(Zigbee, Bluetooth, NFC, RFID, WiFi, LoRa, Ethernet, ModBus etc.) - Knowledge in application Standards for Connected Offers and
(beside other: ETSI EN 300 328; ETSI EN 301 489; ETSI EN 300 330; IEC 62311) - Basic knowledge in Cyber Security
(beside other: IEC 62443) - Mastering English language is mandatory
- This position also requests soft skills such as: Organized, rigorous, diplomat and pedagogue. You need to be able to come to compromises, but you can push strongly when required, to ensure the compliance of our offers and systems.
时间表: 全职
请求编号: 007VL6