Maintenance release of EcoStruxure Machine Expert – HVAC (V1.7.0), with implementation of new features and bug fixing. NEW FEATURES IN TM173O***** (FIRMWARE MSK 825.03) • Improve USB pendrive management • Improve Watch Dog management • Updated Menu BIOS • Updated Retain area management: data saved into flash memory at device power off (area reduced to 0…384 Bytes) (1) New flash memory area managed through target variable sysRetainPars (1) 384 RETAIN area, 7680 Bytes sysRetainPars area Introducing a new product in our HVAC portfolio, designed to not only replace the TM171O Optimized Logic Controller family but also provide functionalities comparable to the TM172P Optimized and Performance Logic Controllers family. With features like CAN and USB connectivity, this product is ideal for controlling small Air Handler Units, Dryers, Boilers, and Process Chillers NEW FEATURES IN TM172P*****/TM172O***** (FIRMWARE MSK 596.14 AND MSK 668.14) • Improve BACnet MSV to have 10 states. • Add the forwarding of message MODBUS 06 in the bridge. • Connection password to enable for added security. • Additional Modbus Functions (@200).