我们的品牌

欢迎访问施耐德电气网站

欢迎访问我们的网站。
Accessory, Network Management Cards, USB to Dry Contact Accessory, for Network Management Cards, provides one dry contact input and two relay outputs

AP9811

Connect the host device of a Network Management Card 3 with peripheral devices
The USB to Dry Contact Accessory connects to the USB port on your NMC.
Through the NMC Web UI, specify which alarms will cause a change in the state of each relay output.
Set the actions that will occur at the host due to a change in state of your input device.
Environmental Data
Use Better
回收纸板包装
information_stroke
回收的纸板含量至少为70%(美国为50%)。一些订单可能包括非回收纸板,直至库存耗尽。
能效优化
information_stroke
本产品的能效比市场平均值或上一代产品节能率至少高10%。
高能效产品
Use Again
回收
information_stroke
产品是否已纳入全球收回计划。某些产品在某些地区可以购买,请验证您所在的国家是否有此类产品。
不支持

需要更多信息?点击下方按钮查看更多常见问题

轻松找到该产品常见问题解答