欢迎访问施耐德电气网站

欢迎访问我们的网站。

您可以选择其他国家/地区以查看可用产品或转至我们的全球网站了解公司信息

选择其他国家或区域

  • Default Alternative Text
    Open Road Tolling system that provides class leading revenue collection, improves traffic congestion and optimizes operations & maintenance.

    Tolling Management Solution

  • 收费管理解决方案

    施耐德电气交通开放道路收费系统提供了同级领先的税收征管、改善交通拥堵,同时优化运营和维护。

网络数据中心内的两个人正在观看笔记本电脑

Challenges

Our world population is growing at fast rate. As a result, transportation agencies across the globe are facing increasing challenges managing traffic congestion and throughput, while creating an environment that promotes safe and efficient commutes and the reduction of travel times and CO2 emissions.
Normal cars racing on a race track.

Schneider Electric Open Road Tolling Solution

Value Proposition

  • 向上图标

    Making Tolling more Efficient, Safe and Sustainable

  • Handshake icon

    30+ Years of Experience in Tolling

事实

  • Blue automotive icon 机动车复合平均增长率(CAGR)为3%,这一增长率至少将延续到2030年。
  • Blue earth icon 到2050年世界人口将增长34%。
  • Blue smart city icon 到2050年世界人口的70%将居住在城市。
  • Blue asset optimisation 系统准确性达到99.9%。
  • Default Alternative Text 系统24/7全天候可用。
  • 蓝色树叶图标 交通拥堵现象减少20%。