在Premium的模拟量输入模块TSXAEY800中,如何使用输入滤波的功能?
问题描述:
如何在Premium的模拟量输入模块AEY800中使用输入滤波的功能?所属产品线:
Modicon Premium解决方法:
在AEY800的配置菜单中,对每个通道都有滤波功能设置,0-6的滤波功能分别对应的滤波响应时间和干扰信号如下:
| Filtering values are as follows: | ||||
| Desired Efficiency | Required Value | Corresponding | Filter Response Time at 63% | Cut_off Frequency (in Hz) |
| No filtering | 0 | 0 | 0 | 0 |
| Low filtering | 1 2 | 0,750 0,850 | 100ms 202ms | 1,591 0,788 |
| Medium filtering | 3 4 | 0,937 0,969 | 419ms 851ms | 0,79 0,187 |
| High filtering | 5 6 | 0,984 0,992 | 1.714ms 3.442ms | 0,093 0,046 |
用户根据应用进行选择。
是否有帮助?