[Q&A]ATV212如何用MODBUS通讯查看当前故障状态?
通过Modbus查看地址FC90的值可以判断出当前故障
Code Value Value Description
NEr r 0 No error]
OC1 1 [Over-current during acceleration]
OC2 2 [Over-current during deceleration]
OC3 3 [Over-current during constant speed operation]
OCL 4 [Over-current in load at startup]
OCA 5 [Short circuit in arm]
EPH I 8 [Input phase failure]
EPHO 9 [Output phase failure]
OP1 A [Overvoltage during acceleration]
OP2 B [Overvoltage during deceleration]
OP3 C [Overvoltage during constant speed operation]
OL1 D [Over-LOAD in inverter]
OL2 E [Over-LOAD in motor]
OH 10 [Overheat trip]
E 11 [Emergency stop]
EEP1 12 [EEPROM fault 1] (writing operation)
EEP2 13 [EEPROM fault 2] (reading operation)
EEP3 14 [EEPROM fault 3] (other)
Err2 15 [RAM fault]
Err3 16 [ROM fault]
Err4 17 [CPU fault]
Err5 18 [Communication error trip]
Err7 1A [Current detector fault]
Err8 1B [Optional circuit board type error]
Err9 1C [Graphic keypad communication error]
UC 1D [Small-current trip]
UP1 1E [Trip due to undervoltage in main circuit]
Ot 20 [Over-torque trip]
EF2 22 [Ground fault trip] (hardware detection)
OC1P 25 [Overcurrent flowing in element during acceleration]
OC2P 26 [Overcurrent flowing in element during deceleration]
OC3P 27 [Overcurrent flowing in element during operation]
EtYP 29 [Inverter type error]
OH2 2E [External thermal input]
SOUt 2F [VIA cable break]
E-18 32 [Break in an analog signal cable]
E-19 33 [CPU fault]
E-20 34 [Excess torque boost]
E-21 35 [CPU fault]
Etn1 54 [Auto-tuning error]
Fd1 48 [Closed damper 1 fault]
Fd2 49 [Closed damper 2 fault]。
是否有帮助?