我们的品牌

欢迎访问施耐德电气网站

欢迎访问我们的网站。
		
我们今天能为您提供什么帮助?
M340使用以太网转MB+网关TCSEGDB23F24FA做Peer Cop全局数据通讯无数据
所属产品线:
工业以太网交换机

解决方法:

M340或M580使用以太网转MB+网关TCSEGDB23F24FA做Peer Cop特定数据通讯方式正常,全局数据通讯方式时无数据收发,此情况是因为MB+网关TCSEGDB23F24FA在做Peer Cop全局数据通讯方式时需要占用自%MW3072开始的12个字,所以M340或M580在分配地址内存%MW区时至少要到%MW3084,Peer Cop全局数据通讯方式才能正常通讯!

Configure the M340 CPU PLC memory to accommodate 2048 %M IO bits plus the
number of inputs required for your application and 3084 %MW words. For %MW
words, there is 1024 words for the input registers between the default starting offset
of 2048 and the starting default offset for Peer Cop Health 3072+12 words. You can
adjust these values to your application as required.
Peer Cop Health writes 12 words to the M340 CPU starting by default at %MW3072. To accommodate the Health block at this default location, configure the CPU for a minimum of %MW3084 words. If these 12 words are not configured in the CPU and reserved for the Health block, Peer Cop and Global Data services are disabled on Modbus Plus.