我们的品牌

欢迎访问施耐德电气网站

欢迎访问我们的网站。
		
我们今天能为您提供什么帮助?
M340的Modbus端口在用READ_VAR和WRITE_VAR指令时,分别支持什么Modbus功能代码?相同的指令在Quantum和Premium中呢?
问题描述:
M340的Modbus端口在用READ_VAR和WRITE_VAR指令时,分别支持什么Modbus功能代码?相同的指令在Quantum和Premium中呢?

所属产品线:
Modicon Quantum

解决方法:

READ_VAR和WRITE_VAR在M340中支持的Modbus功能代码为:

Modbus request Function code Communication function
Read bits 16#01 or  16#02 READ_VAR
Read words 16#03 or  16#04 READ_VAR
Write bits 16#0F WRITE_VAR
Write words 16#10 WRITE_VAR

READ_VAR和WRITE_VAR在Premium中支持的Modbus功能代码为:

Modbus request Function code Communication function
Read bits 16#01 READ_VAR
Read words 16#03 READ_VAR
Write one or n  bits 16#05 or 16#0F WRITE_VAR
Write one or n  words 16#06 or 16#10 WRITE_VAR
Read input bits* 16#02 SEND_REQ
Read input words* 16#04 SEND_REQ
*except on Terminal port

Quantum中的XXMIT支持的Modbus功能代码为:

Function Code Master PLC Data Area Slave PLC Data Area
03 (Read multiple 4x) %MW (destination) %MW (source)
04 (Read multiple 3x) %MW (destination) %IW (source)
01 (Read multiple 0x) %M (destination) %Q (source)
02 (Read multiple 1x) %M (destination) %I (source)
16 (Write multiple 4x) %MW (source) %MW (destination)
15 (Write multiple 0x) %M (source) %Q (destination)
05 (Write single 0x) %M (source) %Q (destination)
06 (Write single 4x) %MW (source) %MW (destination)