Vijeo Citect与三菱PLC通信时,端口与板的设置该注意些什么?
问题描述:
Vijeo Citect与三菱PLC通信时,端口与板的设置该注意些什么?所属产品线:
AVEVA™ Plant SCADA解决方法:
Board Name: Board1
Board Type: TCPIP
Address: 0
Port Name: Port1_Board1
Board Name: Board1
Special Opt: -i192.168.0.21 -P1025 -T (IP address of the PLC)
IODevice Name: IODeviceName
Address: 255
Protocol: MELSCNET1
PortName: Port1_Board1


是否有帮助?