Citect 7.3和7.4版本的多语言切换怎样配置?
问题描述:
Citect 7.3和7.4版本的多语言切换怎样配置?所属产品线:
AVEVA™ Plant SCADA解决方法:
下面以中英文切换举例
1,画面上的文本写成“@(文本)”,所有需要显示多语言的文本,都要加@符号,此处的文本需要填写英文。
2,工程编辑器--System—Languages,把要翻译的语言加进去,如添加简体中文如下图,所有要显示的语言,都要在这里添加

3,保存画面并编译。编译之后,会在工程文件夹中Chinese(Simplified,PRC).dbf(对应语言)的Native一列里出现加了@的文字,然后在Local一栏加上对应的中文翻译,保存,编译。
4,触发多语言切换,可通过cicode。代码如下,如果不写代码可以登录一个用户并选择语言即可,以下仅供参考:
INT
FUNCTION
LoginAndSetLanguage(STRING sLanguage, INT nCharSet )
INT nStatus;
nStatus = Login ("kernel", "kernel" , 0, sLanguage );
RETURN nStatus;
END
是否有帮助?