SoMachine Basic V1.6自定义功能块%UDFB如何添加模拟量输入输出参数?
所属产品线:
EcoStruxure Machine Expert - Basic(原SoMachine Basic)解决方法:
SoMachine Basic V1.6中新加了自定义功能块%UDFB功能,在SoMachine Basic软件中编程-任务-用户定义功能块-新建UDFB1_,添加布尔输入输出,定义参数%PARAM0、%PARAM1,主任务中POU直接调用即可。布尔输入输出能直接显示在调用的功能块%UDFB1_1输入输出管脚上,但是参数%PARAM0、%PARAM1不会出现在调用的功能块%UDFB1_1输入输出管脚上,要在主任务中POU中使用操作块给参数%PARAM0、%PARAM1赋值,如%MW100:=%UDFB1_1.PARAM0和%UDFB1_1.PARAM1:=%MW200。
是否有帮助?