Citect 7.X冗余双网卡报警服务器一台运行正常,另外一台卡在Starting状态无法运行?
Citect 7.X冗余双网卡报警服务器其中一台运行正常,另一台卡在Starting状态无法运行,提示信息显示“initialize functions”。出现此故障的原因是4个网卡的IP地址设定在了同一个子网段内,例如:
1. Name: PrimaryLAN1, Address: 192.168.0.1
2. Name: StandbyLAN1, Address: 192.168.0.2
3. Name: PrimaryLAN2, Address: 192.168.0.3
4. Name: StandbyLAN2, Address: 192.168.0.4
这种设定方式需要Citect 7.5 SP1 Patch 9及以上的版本冗余双网卡报警服务器才能正常运行,否则就会出现上述情况,建议使用如下配置示例:
Project Editor > Network Addresses
1. Name: PrimaryLAN1, Address: 192.168.0.1
2. Name: StandbyLAN1, Address: 192.168.0.2
3. Name: PrimaryLAN2, Address: 10.0.0.1
4. Name: StandbyLAN2, Address: 10.0.0.2
Project Editor > Servers > Alarm Servers
1. Name: PriAlarmServer, Mode: Primary, Network Addresses: PrimaryLAN1,PrimaryLAN2
2. Name: StaAlarmServer, Mode: Standby, Network Addresses: StandbyLAN1,StandbyLAN2
(Note that Network Addresses order is important)
是否有帮助?


需要帮助?
产品选型工具
快速轻松地为您的应用找到合适的产品和附件。
获取报价
开启在线采购咨询,我们的专家将与您联系。
我要采购
开始在线采购咨询,专家将会与您联系!
帮助中心
一站式查找满足您所有需求的支持资源。