我们今天能为您提供什么帮助?

M340 的CPU的芯片参数什么?主频是多少?

所属产品线:
Modicon M580 ePAC

解决方法:

The all M340 processors are from ARM9 family and the core processor is a 32 bits processor. Its speed is 180MHz except for BMXP341000


The speed of BMXP341000 is 110 MHz..