通过FTP方式访问M580时,为什么会出现报错421 Service not available,closing control connection?
问题描述:
通过FTP方式访问M580时,为什么会出现报错421 Service not available,closing control connection?所属产品线:
Modicon M580 ePAC原因:
第一,M580安全性中要未启用FTP功能;第二 CPU的固件要低于SV2.0;第三,用户名和密码输入错误。解决方法:
第一,M580安全性中要启用FTP功能;第二 CPU的固件要高于SV2.0;第三,正确输入用户名和密码。
是否有帮助?