Citect字符串如何比较?
问题描述:
Citect字符串如何比较?所属产品线:
AVEVA™ Plant SCADA解决方法:
CITECT 字符串比较使用StrComp()函数,需要注意的是,字符串比较有两种方式:1 二进制方式比较(转换成ANSI编码进行比较);2 文本模式比较(字符比较,不区分大小写)。使用此函数比较之前要声明比较方式,详见如下示例:
Example
Option Compare Binary
Dim vntResult as Variant
vntResult = ("CitectVBA rules!", "Citectvba Rules!")
' returns 1 (strings unequal) Example
Option Compare Text
Dim vntResult as Variant
vntResult = ("CitectVBA rules!", "Citectvba Rules!")
' returns 0 (strings equal) 定义成STRING类型时是采用转换成ANSI编码进行比较的,详见如下示例:
Return Value
Returns a variant containing an integer data type indicating the result of the string compare:
-
Returns -1 where String1 is less than String2.
-
Returns 0 where String1 is equal to String2.
-
Returns 1 where String1 is greater than String2.
-
Returns Null where String1 or String2s Null.
Example
Dim strTest1 as String Dim strTest2 as String Dim strTest3 as String Dim vntComp strTest1 = "ABCD" strTest2 = "abcd" strTest3 = NULL vntComp = StrComp(strTest1, strTest2) ' Returns -1 (less than) vntComp = StrComp(strTest1, strTest1) ' Returns 0 (equal to) vntComp = StrComp(strTest2, strTest1) ' Returns 1 (greater than) vntComp = StrComp(strTest1, strTest3) ' Returns NULL (strTest3 is NULL)
是否有帮助?