怎样在Citect上使用Combobox控件?
There are 2 ways to do it, Use:
* ActiveX combo box, or
* ciText.combobox.
To use an ActiveX combo box:
Paste the activeX control “Microsoft Forms 2.0 ComboBox” on a graphics page
Associate the TEXT property with a Tag. This tag will contain the value of the item selected from the ComboBox.
FUNCTION MyPageLoad()
OBJECT oComboBox1
INT iIndex
oComboBox1 = ObjectByName("AN210")
_ObjectCallMethod(oComboBox1,"Clear")
_ObjectCallMethod(oComboBox1,"AddItem","Tag1",iIndex)
iIndex = iIndex + 1
_ObjectCallMethod(oComboBox1,"AddItem","Tag2",iIndex)
iIndex = iIndex + 1
_ObjectCallMethod(oComboBox1,"AddItem","Tag3",iIndex)
END
FUNCTION MyPageLoad2()
OBJECT oComboBox1
INT iIndex
oComboBox1 = ObjectByName("AN210")
_ObjectCallMethod(oComboBox1,"Clear")
_ObjectCallMethod(oComboBox1,"AddItem",Tag1,iIndex)
iIndex = iIndex + 1
_ObjectCallMethod(oComboBox1,"AddItem",Tag2,iIndex)
iIndex = iIndex + 1
_ObjectCallMethod(oComboBox1,"AddItem",Tag3,iIndex)
iIndex = iIndex + 1
END
To use a ciText combo box:
1. Use example project
2. Paste the following function to Recipe.Ci file
3. Configure a device using DBF file type (as we are using Example project, Recipe.dbf already exists)
4. Insert CiText.ComboBox on a graphics page (Say page "Recipe")
5. Find out the animation point occupied by this control
6. Add a button on this page as well and call the following function in the command field LoadRecipe2ComboBox("AN35")
7. Compile the project
8. Run the project
FUNCTION LoadRecipe2ComboBox(STRING sAN)
STRING sName;
OBJECT oComboBox1;
INT iComboBoxIndex1 = 0;
INT iRecNo;
IF hRecipe < 0 THEN
hRecipe = DevOpen("Recipes", 0);
END
IF hRecipe >= 0 THEN
iRecNo = DevRecNo(hRecipe); !Current Record Number
DevSeek(hRecipe, 1);
oComboBox1 = ObjectByName(sAN);
_ObjectCallMethod(oComboBox1, "Clear");
WHILE NOT DevEOF(hRecipe) DO
sName = DevGetField(hRecipe, "Name");
_ObjectCallMethod(oComboBox1, "AddItem", sName,
iComboBoxIndex1);
iComboBoxIndex1 = iComboBoxIndex1 + 1;
DevNext(hRecipe);
END
DevSeek(hRecipe, iRecNo); // Reinstate the original position
ELSE
Message("ComboBox", "Cannot Open Recipes.DBF device.", 0);
END
END
If you want to use the function with other applications, you should modify it accordingly. For example, if you have more than one ComboBox on a page, you could code the function as generic one as shown below. Simply pass the device handle, animation point number and data field name. Note that you want the function to be call on page entry, you have to delay the call until the control is instantiated. In V6, a new page event called "On page shown" is introduced that guarantee all objects are instantiated. Hope this would help.
FUNCTION LoadRecipe2ComboBox(INT hRecipe, STRING sAN, STRING sFieldName)
STRING sName;
OBJECT oComboBox1;
INT iComboBoxIndex1 = 0;
INT iRecNo;
IF hRecipe >= 0 THEN
iRecNo = DevRecNo(hRecipe); !Current Record Number
DevSeek(hRecipe, 1);
oComboBox1 = ObjectByName(sAN);
_ObjectCallMethod(oComboBox1, "Clear");
WHILE NOT DevEOF(hRecipe) DO
sName = DevGetField(hRecipe, sFieldName);
_ObjectCallMethod(oComboBox1, "AddItem", sName,
iComboBoxIndex1);
iComboBoxIndex1 = iComboBoxIndex1 + 1;
DevNext(hRecipe);
END
DevSeek(hRecipe, iRecNo); // Reinstate the original position
ELSE
Message("ComboBox", "Cannot Open Recipes.DBF device.", 0);
END
END
是否有帮助?


需要帮助?
产品选型工具
快速轻松地为您的应用找到合适的产品和附件。
获取报价
开启在线采购咨询,我们的专家将与您联系。
我要采购
开始在线采购咨询,专家将会与您联系!
帮助中心
一站式查找满足您所有需求的支持资源。