PM2125C仪表支持哪些标准报警?
问题描述:
PM2125C仪表支持哪些标准报警?所属产品线:
PM2000解决方法:
PM2125C仪表可支持以下14种标准报警:
| 报警标签 | |
| Over Phase Current | 过流,相电流 |
| Under Phase Curren | 欠流,相电流 |
| Over Voltage L-L | 过压,线电压 |
| Under Voltage L-L | 欠压,线电压 |
| Over Voltage L-N | 过压,相电压 |
| Under Voltage L-N | 欠压,相电压 |
| Over Active Power | 过功率,有功 |
| Over Reactive Power | 过功率,无功 |
| Over Apparent Power | 过功率,视在 |
| Leading True PF | 超前的PF |
| Lagging True PF | 滞后的PF |
| Over Frequency | 过频率 |
| Under Frequency | 低频率 |
| Over Voltage THD | 过电压THD |
是否有帮助?