[Q&A]Machine Expert 程序编译时,编译器错误代码C0044的原因及处理方法?
问题描述:
Machine Expert 程序编译时,编译器错误代码C0044处理方法所属产品线:
EcoStruxure Machine Expert(原SoMachine)解决方法:
Machine Expert 程序编译时,编译器错误C0044的消息,错误原因,解决方法,错误示例如下:
弹出消息
Assignment to input is missing for parameter ‘<input variable name>’ in call of ‘<function block name>’
错误原因
尽管未声明输入变量,但依然传送了参数。
解决方法
声明输入变量。
错误示例
PROGRAM PLC_PRG
VAR
inst : FB;
END_VAR
inst(1);
FUNCTION_BLOCK FB
VAR_INPUT
END_VAR
--> C0044: Assignment to input is missing for parameter '1' in call of 'FB'
错误纠正
FUNCTION_BLOCK FB
VAR_INPUT
in : INT;
END_VAR
是否有帮助?