M200、M221等PLC的定时器功能块TON、TOF可以实现累计计时吗?
问题描述:
M200、M221等PLC的定时器功能块TON、TOF可以实现累计计时吗?所属产品线:
EcoStruxure Machine Expert - Basic(原SoMachine Basic)应用环境:
EcoStruxure Machine Expert - Basic解决方法:
可以,勾选相应定时器的“保持”后,其IN管脚断开时,定时器的当前值不会归0,IN管脚再次接通时,定时器会从保持的上次计时值开始计时,而不是从0开始。如下图:

是否有帮助?