我们今天能为您提供什么帮助?

Vijeo Designer随着SoMachine或EcoStruxure Machine Expert V1.1(或更早版本)安装的,但无法安装Vijeo Designer 6.2 SP9,怎么办?

问题描述:
无法在装有SoMachine或EcoStruxure Machine Expert的PC上安装Vijeo Designer 6.2 SP9补丁包解决办法

所属产品线:
Vijeo Designer

解决方法:

在安装了SoMachin V4.X或EcoStruxure Machine Expert 1.1(包含V1.1之前版本)的PC上安装Vijeo Designer的Service Pack 9.x,我们将看到以下错误:

此错误表明,当电脑上安装了SoMachine V4.X或者EcoStruxure Machine Expert 1.1(包括V1.1更早版本),我们无法在Vijeo Designer上安装Service Pack 9的补丁包。这是因为Vijeo Designer的Service Pack 9集成了一个与旧版本不兼容的新版本Codesys,Service Pack 9的补丁包的Codesys适用于EcoStruxure Machine Expert V1.2和更高版本。

如果电脑已经装了SoMachine V4.X或者EcoStruxure Machine Expert 1.1(包括V1.1更早版本),但又需要使用vjeo Designer 6.2的Service Pack 9的版本,建议在虚拟机里安装独立版本的Vijeo Designer 6.2。