我们今天能为您提供什么帮助?

LXM32M的DTM中的Start the Motion & Continue the Motion 是什么意思?

问题描述:
我们无法在LXM32M的DTM帮助中找到关于Start the Motion & Continue the Motion的任何说明

所属产品线:
Lexium 32

应用环境:
LXM32M,DTM,Somove

原因:
文档缺失

解决方法:

在当前的LXM32 DTM中,我们注意到在控制面板中有3个关于“Motion squence”的选项。

但是在线帮助只解释了其中一个选项

Start the Motion & Continue the Motion 的具体解释如下:

With the selection “Start the Motion” and pressing the button “START” you start the sequence with the data set number defined in the textbox DATSET.
-With the selection
Continue the Motion and pressing STARTyou start the next dataset within your sequence, when the dataset is waiting for the defined transition condition.
So it continues your defined sequence.
For example if you
´ve defined daset number 0 with transition condition Rising Edge. Movement of dataset 0 is finished, (next dataset would be 1) and its waiting for the transition condition.