如何在Vijeo Designer Basic设置触摸屏HMIGXU5512的IP地址?
问题描述:
如何在Vijeo Designer Basic设置触摸屏HMIGXU5512的IP地址?所属产品线:
Vijeo Designer Basic解决方法:
用Vijeo Designer Basic 可以给触摸屏HMIGXU5512设置IP地址,IP地址可以根据需要修改,设置步骤如下:
1.在Vijeo Designer Basic建String类型的内部变量,名字为STRING01,“数据细节”中字节长度设20


2.在画布上放置一个开关按钮,在“常规”选“点击时” “设置IP地址”,关联变量STRING01

3.在画布放置一个字符串显示控件,关联变量STRING01、显示长度设置20、将“启用输入模式”打钩、把“输入模式”选项中的“显示弹出键盘”改成“十进制键盘”


4.在“网络”选项卡的“允许在Run time设置IP地址”前打钩

5.编译并下载程序到触摸屏HMIGXU5512,在数值显示控件里输入IP地址,点击赋有改变IP功能的按钮,触摸屏的IP地址会发生改变
是否有帮助?