我们今天能为您提供什么帮助?

EcoStruxure Control Expert V14卸载,再安装Unity Pro V13.1,软件打开会报错?

问题描述:
软件打开报错

所属产品线:
EcoStruxure Control Expert(原Unity Pro)

解决方法:

Win10系统安装Control Expert V14后再卸载,然后安装Unity Pro V13,安装过程中未报错,但是打开Unity报如下错误

如果点击OK建立工程报“Unity has tried to read from a virtual address or to write to a virtual address for which unity has no access.”

建议按如下方式操作:

  • 卸载已安装的Unity Pro V13.1
  • 手动删除以下文件:

C:\Program Files(x86)\Common Files\Schneider Electric Shared\RAT
C:\Program Files(x86)\Common Files\Schneider Electric Shared\SRCSDK
C:\Program Files(x86)\Common Files\Schneider Electric Shared\SSTA

  • 重启计算机,重新安装Unity  Pro V13.1