我们今天能为您提供什么帮助?

如何用Vijeo Designer Basic 2.0将数据以表格形式记录并显示?

问题描述:
如何用Vijeo Designer Basic 2.0将数据以表格形式记录并显示?

所属产品线:
Vijeo Designer Basic

解决方法:

使用Vijeo Designer Basic 2.0的“数据记录”控件可以将数据以表格形式记录与显示。如用表格记录电机电流、电机温度、电机电压、电机转速等参数,画面如下:


操作步骤:
1.把Vijeo basic 2.0 的菜单“画图”——“数据记录表”拖到画面上,在“属性列”——“数据”——“数据量”设4,调整列宽,本例设置为100


2. 在导航窗口“数据记录”新建记录组LoggingGroup01,属性中取样设置为“周期的”,单位设置为“秒”,变量存储器选“SRAM”数据被记录到触摸屏中断电可保持,若要保存到U盘中,变量存储器选“SRAM文件”


3. 按下图新建变量,变量关联记录组LoggingGroup01



4.做4个数值输入控件关联变量电机电流、电机温度、电机电压、电机转速,将程序传输到触摸屏,当这些数据发生变化时会被记录到表格中。点击表头变量弹出筛选对话框,可以根据需求筛选要显示的数据