我们今天能为您提供什么帮助?

Vijeo Designer Basic可以与施耐德PLC做Modbus RTU模拟吗?

问题描述:
Vijeo Designer Basic可以与施耐德PLC做Modbus RTU模拟吗?

所属产品线:
Vijeo Designer Basic

解决方法:

施耐德触摸屏软件Vijeo Designer Basic可以与施耐德PLC做Modbus RTU模拟。将PLC通过USB转RS485电缆连接到电脑的USB口上,修改该端口编号为2,然后用电脑来模拟触摸屏监视或控制外部变量的值。

修改端口编号的步骤:

在电脑的“设备管理器”——“端口(COM和LPT)”选中被识别的USB转RS485的电缆,点右键"属性"——“端口设置”——“高级”——将COM端口号改成COM2:

以M200 PLC为例,在Machine Expert Basic设置MODBUS为从站:

在Vijeo Designer Basic建驱动ModbusRTU选择COM2口:

在Vijeo Designer Basic点“启动模拟(S)(生成)”即可用电脑模拟触摸屏监视外部变量。